Technical FAQs

Ask a Question

What is the AIR for JD breakers?

Product Line:
Circuit Breakers

Resolution:
For Powerpact J Frame Circuit Breakers, the JD version has the following AIR:
25 kA @ 240 Vac
18 kA @ 480 Vac
14 kA @ 600 Vac
Was this helpful?
What can we do to improve the information ?