Technical FAQs

Ask a Question

What is the Depth of the QMB Fusible panels?

Per catalog section 4620CT9601, Page 3.  The Nema 1 are all 11.50`` deep. (If the trim is provided with a door, the box will be 18`` deep. Factory assembled only.) Nema 3R are 14.90`` deep.



CTA-ID : 2035392
Was this helpful?
What can we do to improve the information ?