Technical FAQs

Ask a Question

What is the catalog number for the replacement lugs of FHL3600015M, 150 amp automatic molded case switch?

Issue:
What is the catalog number for the replacement lugs of FHL3600015M, 150 amp automatic molded case switch?

Product Line:
FHL 150A Molded Case Switches

Environment:
This applies only to the 150A FHL Molded Case Switch. 

Cause:
Need to replace the lugs on a 150A FHL switch.

Resolution:
AL150FA the kit contains 3 lugs.


CTA-ID : 2029576
Was this helpful?
What can we do to improve the information ?