Technical FAQs

Ask a Question

Do we offer a option to supply 120 volts for the logic inputs on the ATV61 and ATV71?

Issue:
Do we offer a option to supply 120 volts for the logic inputs on the ATV61 and ATV71?

Product Line:
Atlviar ATV61 and ATV71

Environment:
All

Cause:
Needs to have an option to supply 120 vac to turn on the logic inputs to start up the drive.

Resolution:
Yes,  The 115 VAC logic input adaptor is part number VW3A3101.

CTA-ID : 2029683
Was this helpful?
What can we do to improve the information ?