Technical FAQs

Ask a Question

Can the two coils of a D-Line reversing contactor be mixed with AC on one side and DC on the other?

No, they can`t be AC on one and DC on the other because the DC coil is so much larger it won`t allow interlocking.

CTA-ID : 2029554
Was this helpful?
What can we do to improve the information ?