Technical FAQs

Ask a Question

What is the catalog number for a terminal cover for use with the US Mounting Bases for the UL489 Multi 9 Circuit Breaker?

The USMBTC is the terminal cover for US mounting bases which provides IP20 ingress protection per IEC 60529; suitable for jumper bars or cable.

CTA-ID : 2029117
Was this helpful?
What can we do to improve the information ?