Technical FAQs

Ask a Question

Is 480-volt control an option for the Tesys U-Line starters?

No the following control voltages are available:
24 vdc - code BL.
24 vac - code B.
48 to 72 vdc - code ES.
48 vac - code ES.
110 to 240 vdc - code FU.
110 to 240 vac - code FU.


CTA-ID : 2028833
Was this helpful?
What can we do to improve the information ?