Technical FAQs

Ask a Question

How does the pullout of the FP221R, Series G01 unit get removed, it is difficult to pull out?

Issue:
Product Design Features

Product Line:
Air Conditioning Disconnects

Environment:
Removing the Pull-out

Cause:
Maintenance or disconnecting

Resolution:
The FP221R is an Obsolete A/C disconnect. To remove the pull-out, one would need to firmly grab the handle on the end of the pullout and pull straight forward. If it appears to be hard, maybe try to slightly rock the pullout "side to side" or "up and down" while pulling.




 
Was this helpful?
What can we do to improve the information ?