Technical FAQs

Ask a Question

What are the current ranges of the RM4JA32F.

What are the contact ratings of 9001KA contact blocks?

Product Line:
30mm Push

9001K/SK/KX 30mm Push Buttons

Confirm the rating of the contact block for an application.                                                          

The 9001 KA contacts are rated NEMA A600. The maximum AC voltage is 600VAC and the maximum thermal current is 10 amps.
9001 KA contacts are also rated NEMA Q600. The maximum DC voltage is 600VDC and the maximum thermal current is 2.5 amps.
Was this helpful?
What can we do to improve the information ?