Technical FAQs

Ask a Question

Can I use LDR type wireway with conduit to individually mounted meterbases? Does this product line have conduit holes pre cut?

Issue:
Can I use LDR type wireway with conduit to individually mounted meterbases?   Does this product line have conduit holes pre cut?

Product Line:
Wireway.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
LDR type NEMA 3R wireway can be used with individual metering. Holes in the wireway are not pre-cut. User will have to cut his own holes.


CTA-ID : 2029106
Was this helpful?
What can we do to improve the information ?