Technical FAQs

Ask a Question

What is the standard lug wire size for QMJ366 fusible switch?

Issue:
Terminal lug data

Product Line:
QMJ Safety Switches

Environment:
Lug wire size

Cause:
Application

Resolution:
The standard terminal lug data for the QMJ366 is (2) 3/0 - 600kcmil Al/Cu wire per phase.
NOTE: There are NO alternate lugs for different wire sizes or quantity's for this switch.




CTA-ID : 2028879
Was this helpful?
What can we do to improve the information ?