Technical FAQs

Ask a Question

Can the Tesys LRD__, LR3D__ or LR9D__ overloads be supplied with two normally open control circuit contacts?

No, these overloads are only available with one normally open and one normally closed control contacts.


CTA-ID : 2029082
Was this helpful?
What can we do to improve the information ?