Technical FAQs

Ask a Question

What is the terminal lug data for DTU326R, series A1 Double Throw Safety Switch?

Issue:
Product Design features

Product Line:
Double Throw Safety Switches

Environment:
Lug wire size

Cause:
Installation

Resolution:
The lugs on this device will accept (2) #250 - 500 kcmil aluminum or copper per phase.

THERE ARE NO ALTERNATE LUGS AVAILABLE

 
Was this helpful?
What can we do to improve the information ?