Technical FAQs

Ask a Question

What does factory modification Y534 represent on the Class 8539 Type S combination starter?

Substitutes FAL circuit breaker for the standard GJL circuit breaker. This modification is only valid for NEMA size 0, 1 & 2 combination starters.


CTA-ID : 2029272
Was this helpful?
What can we do to improve the information ?