Technical FAQs

Ask a Question

Is it possible to obtain 30 mm or push to test type pushbuttons on Compac starters, used on Model 6 Motor Control Centers (MCC`s)?

Issue:
Is it possible to obtain 30 mm or push to test type pushbuttons on Compac starters, used on Model 6 Motor Control Centers (MCC`s)? 

Product Line:
Model 6 motor control centers.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
No. Because of space restrictions on that smaller Compac Starter unit, push to test or 30 mm devices cannot be installed on these smaller buckets. The standard device used is 22 mm.


CTA-ID : 2029059
Was this helpful?
What can we do to improve the information ?