Technical FAQs

Ask a Question

On busplug catalog number PQ4610GRA, what is meaning of the RA suffix on the end of the catalog number?

Issue:
What is the "RA" suffix on the catalog number PQ4610GRA?

Product Line:
I-Line Busway and accessories

Environment:
Selection of busway plug in units.

Cause:
Clarification of catalog number.

Resolution:
The ``RA`` suffix means that the busplug has factory installed Class R type fuse rejection clips and special lugs, usually copper compression lugs.


CTA-ID : 2029259
Was this helpful?
What can we do to improve the information ?