Technical FAQs

Ask a Question

Does Square D make a single phase combination starter? Fusible with Class R fuse clips?

Product Line:
 
Type S combination starters
 
Resolution:
 
Yes - see Digest for Fusible Disconnect Switch Type, Class R, single phase selection table.


CTA-ID : 2030421
Was this helpful?
What can we do to improve the information ?