Technical FAQs

Ask a Question

Can the contactor be replaced on the Class 8536 Type SF__ Nema Size 4 starter ?

No , because the contactor busbars which mate up to the busbars on the overload are staked into the lower housing of the contactor. These busbars cannot be field added to the contactor. The baseplate will also be incorrect.

CTA-ID : 2030474
Was this helpful?
What can we do to improve the information ?