Technical FAQs

Ask a Question

Are the F-Line Contactors available as reversing units?

Issue:
Can the LC1F contactors be ordered as reversing units?

Product Line:
F-Line Contactors - GIC Product

Environment:
US Product

Cause:
Product Ordering

Resolution:
No, however component selection information is available in the current Digest for field assembly of F-Line reversing units.
These are the general components needed:
Contactors - Quantity Two 
Lugs - Quantity Six
Auxiliary contacts - Quantity Two
Power connections - Quantity One
Mechanical interlock - Quantity One
 
Was this helpful?
What can we do to improve the information ?