Technical FAQs

Ask a Question

Are KA36200 and JDA36200 interchangeable in an I line panel?

Issue:
Are KA36200 and JDA36200  interchangeable in an I line panel?

Product Line:
I line panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Yes they are.  Note: the KA36200 is an obsolete circuit breaker frame.  It can be replaced by the JDA36200.  


CTA-ID : 2029922
Was this helpful?
What can we do to improve the information ?