Technical FAQs

Ask a Question

Can the N150MH main breaker kit and H frame circuit breaker be used on an NF 250A interior?

Issue:
Can the N150MH main breaker kit and H frame circuit breaker be used on an NF 250A interior?

Product Line:
NF panelboards and accessories that are sold and supported in the USA.

Environment:
Application

Cause:
Application of the N150MH kit in a 250A NF panelboard.

Resolution:
Yes. The kit includes 2 deadfronts, one for 100A interior and one for 250A interior.


CTA-ID : 2029939
Was this helpful?
What can we do to improve the information ?