Technical FAQs

Ask a Question

What is the coil burden of a 30 amp 8910DPA?

Issue:
What is the coil burden of a 30 amp 8910DPA?

Product Line:
Definite Purpose Contactors

Environment:
Products sold and used in the United States

Cause:
Identifying Coil Consumption

Resolution:
56VA inrush and 6VA sealed for 2 & 3 pole devices , 109VA inrush and 10VA sealed for 4 pole contactors.


CTA-ID : 2030441
Was this helpful?
What can we do to improve the information ?