Technical FAQs

Ask a Question

What is the coil consumption or burden for the Tesys LC*D** contactors?

Issue:
What is the coil consumption or burden for the Tesys LC*D** contactors?

Product Line:
Tesys Contactors and Overload Relays

Environment:
All Products

Cause:
Product Features

Resolution:
All AC coils for the LC1D40 through LC1D80 3 or 4-pole contactors have an inrush of 200VA for 50 Hertz applications or 220VA for 60Hz.
Sealed values are 20VA for 50 Hertz applications or 22VA for 60 Hertz applications. For 50/60 Hertz coil inrush is 245VA and sealed is 26VA


CTA-ID : 2029994
Was this helpful?
What can we do to improve the information ?