Technical FAQs

Ask a Question

What is the catalog number for the external reset button and shaft for the metal enclosed LE1D starter?

Product Line:
 
Tesys D line Enclosed Contactors and Starters

Resolution:
 
XB5AA86102 is the external reset button with an adjustable shaft that is 17-120mm (0.67 to 4.72 inches).


CTA-ID : 2029801
Was this helpful?
What can we do to improve the information ?