Technical FAQs

Ask a Question

What is the replacement for Merlin Gerin breaker type CJ400N or NSJ400N?

Issue:
What is the replacement for Merlin Gerin breaker type CJ400N or NSJ400N?

Product Line:
Obsolete CJ and NSJ Breakers

Environment:
This includes CJ400N and NSJ400N Molded Case Circuit Breakers

Cause:
Need to replace either the CJ400N o NSJ400N breaker.

Resolution:
Both the CJ400N and the NSJ400N are obsolete along with any of their accessories and have been replaced by the PowerPact L frame breaker.
Converting from the CJ400N to the PowerPact L will involve changes in the mounting, etc. It is not a one for one swap.
Converting from the NSJ400N to the PowerPact L all of the dimensions are the same and many of the accessories are the same as well.

CTA-ID : 2031246
Was this helpful?
What can we do to improve the information ?