Technical FAQs

Ask a Question

Customer needed to know if a LC1F780 can be turned upside down and use the load connections as line connections and the line as load connections?

Yes you can rotate the covers and the markings will be correct then.


CTA-ID : 2031427
Was this helpful?
What can we do to improve the information ?