Technical FAQs

Ask a Question

Is the 115 / 120 volt control coil available as replacement part for the LC1F115 or LC1F150 contactor?

Product Line:
 
Tesys F line Contactors and Accessories
 
Resolution:
 For 60 hertz standard coil code G6 order LX1FF095.

For low sealed consumption coil code G7 (40 - 400 hertz) which offers high tolerance to inrush voltage drops, immune to micro-breaks (main supply or contact chain) and are capable of operation on networks with harmonic numbers less than or equal to 7; order LX9FF127.


CTA-ID : 2031433
Was this helpful?
What can we do to improve the information ?