Technical FAQs

Ask a Question

Is a QO or QOB type breaker available with a 1021 shunt trip that does not take up an extra space in the load center or panel?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
No. The QO breakers must utilize the extra space for the shunt trip. Only the larger molded case breakers have the shunt trip mechanism internal to the breaker itself.
 
Was this helpful?
What can we do to improve the information ?