Technical FAQs

Ask a Question

What is the part number for the internal lexan lever on a 2510MCR3 manual starter?

Product Line:
2510 Manual starter, Type M and Type T

Environment:
NEMA Manual motor starter, 2510M, 2510T

Resolution:
Use a 9998IL1 (eye - el - one)


CTA-ID : 2030552
Was this helpful?
What can we do to improve the information ?