Technical FAQs

Ask a Question

What are the repair parts for a D225N Series E01 General Duty Safety Switch?<br /> <br />

Issue:
Repair parts

Product Line:
GD Safety Switch

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 40510-460-50
Load base assembly - 40510-461-50
Arc suppressor - 40510-310-03
Neutral assembly - 40510-462-50
Base assembly mounting screws - 21427-202-41 (6) required for line base & (7) required for load base.
Arc suppressor mounting screw - 40205-082-01
Neutral assembly mounting screw - 21404-202-00 (2) required
Neutral assembly mounting washer - 23602-117-01 (2) required
Neutral bonding assembly - 40283-185-79
Cross Arm Insulator - 40510-308-01 (insulator) and 40510-318-01 (dust shield - retainer for insulator)




CTA-ID : 2030951
Was this helpful?
What can we do to improve the information ?