Technical FAQs

Ask a Question

What is the warranty period on Schneider Electric Surge Protective Device (SPD) products?

Issue:
Warranty

Product Line:
Surge Protective Devices

Environment:
UL 1449 3rd ed., ANSI/IEEE C62.41 and C62.45

Cause:
A device or component thereof which reaches end-of-life prematurely may be replaced under warranty.

Resolution:
The warranty period for surge protective device components is 10 years, and is handled with participation of Surgelogic personnel.  Warranty covers replacement of the device or component but does not cover labor to replace or dispose of product.


CTA-ID : 2030763
Was this helpful?
What can we do to improve the information ?