Technical FAQs

Ask a Question

Is it possible to obtain a fusible plug-in unit on E-way product selectors? Or, do I enter them as separate line items?

Issue:
Is it possible to obtain a fusible plug-in unit on E-way product selectors?  Or, do I enter them as separate line items?

Product Line:
Busway.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Order as separate line items, fusible plug in units are not on product selectors which specifies lengths of busway run, elbows, etc.


CTA-ID : 2031236
Was this helpful?
What can we do to improve the information ?