Technical FAQs

Ask a Question

What is the difference between a PJA36120 and PJA36120U31A?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment

Resolution:
The PJA36120 does not have an adjustable current setting (long-time), and you cannot replace the trip unit. It is a thermal-magnetic equivalent.
The PJA36120U31A has adjustable long-time, and you can replace the trip unit, and upgrade to greater functionality if desired.


CTA-ID : 2031125
Was this helpful?
What can we do to improve the information ?