Technical FAQs

Ask a Question

Is there a Federal Pioneer NAGF250 ground fault breaker available.

The maximum amperage for an NAGF breaker is 40 amps. The part number is NAGF240. For pool or hot tubs requiring 50 amps we suggest the NAGF250SB. This comes complete with a type 1/3 R rated enclosure, a factory installed 2 pole 50 amp non-automatic GFCI and a loose NCO250 stab-lok circuit breaker that needs to be installed into your FPE loadcenter.

CTA-ID : 2031856
Was this helpful?
What can we do to improve the information ?