Technical FAQs

Ask a Question

What is the DC amperage rating for a 2510 type K*1 manual switch?

Issue:What is the DC amperage rating for a 2510KO1?

Product Line: 2510 type K manual switch

Environment: Products sold and used in the United States

Cause:What is the DC amperage rating for a 2510KO1?

Resolution: We do not publish DC amperage ratings but do publish Hp ratings at various DC voltages. The 2510 KO1 is good for 1 horsepower at 90vDC; 2 horsepower at 115vDC; 1.5 horsepower at 230vDC.


CTA-ID : 2032197
Was this helpful?
What can we do to improve the information ?