Technical FAQs

Ask a Question

What are the repair parts for a CD222N Series F01 General Duty Safety Switch?

Issue:
Repair Parts

Product Line:
General Duty Safety Switch

Environment:
Canadian 

Cause:
Maintenance

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 40566-421-50
Load base assembly - 40560-026-50
Arc shield - 40560-018-01
Mechanism assembly - 40566-378-50
Handle assembly - 40566-387-50
Lockplate - 40566-388-01
Lug assembly - 40251-016-52
Solid neutral assembly - CSN03
Base assembly mounting screw - 40205-160-01 (3) required for line base & (2) required for load base.
Arc shield mounting screw - 40205-145-01
Solid neutral assembly mounting screw - 40205-065-01
Neutral bonding assembly - Contact (888) SQUARED for further assistance.
Lockplate mounting screw - 22999-405-62 (2) required
Cover latch and spring - one each of 40566-072-01 (latch) and 40223-043-01 (spring)


CTA-ID : 2032219
Was this helpful?
What can we do to improve the information ?