Technical FAQs

Ask a Question

What is the Terminal Lug Data for a CD223N General Duty Safety Switch?

Issue:
Product Features

Product Line:
HD Safety Switches

Environment:
Lug wire size and quantity

Cause:
Application

Resolution:

The lugs on this device will accept (1) #12 - 1/0 AWG aluminum or #14 - 1/0 AWG copper conductors per phase. Although the lug will accept #1/0 AWG conductors, the wire bending space available in the switch restricts the maximum to #1 AWG conductors.


CTA-ID : 2032307
Was this helpful?
What can we do to improve the information ?