Technical FAQs

Ask a Question

What is the catalog number for an electrical interlock for the H82345?

Issue:
Accessory

Product Line:
Double Throw Safety Switches

Environment:
Electrical Interlock kit

Cause:
Application

Resolution:
The electrical interlock kit is catalog number EK400DTU2. The kit contains two EIKs, one for each Line base assembly, each with 2NO/2NC contacts, already mounted on a bracket and the complete bracket gets mounted inside the switch. 


CTA-ID : 2031462
Was this helpful?
What can we do to improve the information ?