Technical FAQs

Ask a Question

What kind of mounting hardware would be used on a HCM64TSD or HCM68TSD cover?

Issue:
What kind of mounting hardware would be used on a HCM64TSD or HCM68TSD cover?

Product Line:
I line panelboard.

Environment:
Products sold in the United States.

Cause:
Product featuers.

Resolution:
The correct part number is (18) 40205-130-01 trim screws. Adding a ``K`` to the end of the part number gives them a package of 10.


CTA-ID : 2031774
Was this helpful?
What can we do to improve the information ?