Technical FAQs

Ask a Question

What is the meaning of the suffix on PJA frame breakers ending in CU31A or CU44A?

Product Line:
Circuit Breaker
PowerPact P

Environment:
Electrical Distribution Equipment

Resolution:
The C indicates 100% rated. U31 indicates a standard 3.0 Micrologic trip unit with Long-time and instantaneous functions. U44 indicates a 6.0 Micrologic Ammeter trip unit with long-time, short-time, instantaneous and ground fault functions. "A" indicates type A adjustable rating plug.


CTA-ID : 2032077
Was this helpful?
What can we do to improve the information ?