Technical FAQs

Ask a Question

Is there a kit to add an additional pole to a General Duty, Heavy Duty or Double Throw Safety Switch, (For example make a 2pole into a 3 pole)?

Issue:
Product Design Features

Product Line:
General Duty, Heavy Duty and Double Throw Safety Switches

Environment:
Changing the Poles of the switch.

Cause:
Application

Resolution:
No. There is no kit or accessory that allows an additional Pole to be added to a safety switch. For example, there is no kit to make a 2 pole into a 3 pole or a 3 pole into a 4 pole. This would change the catalog number of the switch and void the UL listing.

 
Was this helpful?
What can we do to improve the information ?