Technical FAQs

Ask a Question

Can the toggle handle on a PowerPact MG or MJ breaker be replaced?

Issue:
Can the toggle handle on a PowerPact MG or MJ breaker be replaced?

Product Line:
PowerPact M and P frame breakers

Environment:
This applies to all PowerPact M frame and to the mechanically operated PowerPact P frame

Cause:
The handle broke off of the breaker can it be replaced?

Resolution:
Only if the extension is all that broke. If the piece affixed to the mechanism is broken, the breaker must be replaced.
The replacement extension is:
Standard Short - S46998
Long - S46996


CTA-ID : 2033162
Was this helpful?
What can we do to improve the information ?