Technical FAQs

Ask a Question

What is the lug wire range on a NJNL36400E20?

Product Line:
Circuit Breakers
Compact NSJ400N

Environment:
Electrical Distribution Equipment

Resolution:
The wire range for the standard lug is (1) #2-600 kcmil copper and (1) #2 to 500 kcmil aluminum.


CTA-ID : 2033172
Was this helpful?
What can we do to improve the information ?