Technical FAQs

Ask a Question

What are the A, B, C, D, E, F, G, H, and J ground fault ampere values for the Micrologic 6.0A, 6.0P, and 6.0H on the 1600A Masterpact breaker NW16H2?

Product Line:
Circuit Breakers

Environment:
Electrical Distribution Equipment.

Resolution:
For all 1200A sensors and greater they are 500A, 640A, 720A, 800A, 880A, 960A, 1040, 1120A, and 1200A respectively.


CTA-ID : 2032543
Was this helpful?
What can we do to improve the information ?