Technical FAQs

Ask a Question

What size is the thermal unit screw for a 2510M or 8536SA, SB or SC?

Part# 21920-16160. That screw is 10-24 by 1/2 pan head flat blade type and comes with the washer.

Note: This part number is (1) screw, order the desired quantity; each pole requires (2) screw assemblies.

CTA-ID : 2032465
Was this helpful?
What can we do to improve the information ?