Technical FAQs

Ask a Question

What is the coil VA rating for the LC1F400 with the LX1FJ*** coils? (Normal 50/60 hertz coils)

Product Line:

Tesys F line Contactors and Accessories
 
Resolution:
 Inrush is 1000 to 1150va and the sealed is 12 to 18va.


CTA-ID : 2032418
Was this helpful?
What can we do to improve the information ?