Technical FAQs

Ask a Question

Does Square D offer the DT362 Double Throw Safety Switch in a NEMA 4X stainless steel enclosure?

Issue:
Product Design Features

Product Line:
Double Throw Safety Switches

Environment:
Enclosure NEMA Rating

Cause:
Application

Resolution:
No, the DT362 is ONLY available in standard steel enclosures.

NOTE: Square D does offer a Unfused Double Throw Safety Switch, catalog number DTU362DS, in stainless if the application permits.


CTA-ID : 2032600
Was this helpful?
What can we do to improve the information ?