Technical FAQs

Ask a Question

What is the external reset mechanism for a current series 8538SGW combination starter?

Qty 1 - 30019-114-66 - Reset sub-assembly (does not include the ring nut listed below but does include 9066 W1 boot)
Qty 1 - 30019-121-01 - Ring nut.
Qty 1 - 9066 W1 - Protective boot (also serves as gasket) (required on NEMA Type 4/4X enclosures).


CTA-ID : 2033676
Was this helpful?
What can we do to improve the information ?