Technical FAQs

Ask a Question

What is the magnetic trip range for a JDL36200

Product Line:
Circuit Breakers
PowerPact J

Environment:
Electrical Distribution Equipment

Resolutions:
Magnetic trip adjustment is 1000 A to 2000 A ,or 5 to 10 times the nominal amperage.


CTA-ID : 2033362
Was this helpful?
What can we do to improve the information ?