Technical FAQs

Ask a Question

What is the coil voltage tolerance for a NEMA contactor/starter?

Issue:     
Identifying coil tolerance of a NEMA coil 

Product Line:
NEMA Contactors and Starters

Environment:
Products sold and used in the United States

Cause:
Identifying acceptable control voltages across a NEMA coil

Resolution:
Per NEMA standards, devices must operate properly from 85% - 110% of nominal voltage


CTA-ID : 2033724
Was this helpful?
What can we do to improve the information ?